Build your symbols with Symbol Editor. This help will get you started quickly.
To draw a line:
To draw a rectangle:
To draw a polyline (connected line segments, closeness not guaranteed):
To undo adding a point, right click. This is doable if the polyline is not finished.
To draw a polygon (connected line segments, closeness guaranteed):
To undo adding a point, right click. This is doable if the polygon is not finished.
To draw a circle:
To draw an ellipse:
An arc is a portion of a circle containing 3 non-linear points.
To draw an arc:
Scheme-it uses quadratic Bézier curve, i.e. 3 points are required.
To draw a curve:
You can extend Line, Arc, and Polyline to make Arrows.
To add text:
To edit text:
To insert an image:
Pins can only placed where coordinates are multiple of 10. For example: (50, 70) is a valid position to place a pin, whereas (51, 70) is not a valid position because its x-coordinate (51) is not a multiple of 10.
To place a pin:
When placed on an object, Symbol Editor will try to bind the pin to that object.
To quickly build a rectangle with pins on it:
In Pin Manager, pins are populated in tabular form. Change a pin and observe immediate change in the canvas.
Elements of a symbol should stay within a rectangle of size 4110x2830 pixels.
The grid make positioning easier. The grid consists of 10x10 squares.
Showing or hiding the grid is optional.
Snap to grid will adjust the receiver of the click to the nearest vertex of the grid squares.
Symbol Editor supports zoom levels from 20% to 400% via a specified scale.
Zoom to fit will try to choose a zoom level so that every element of the symbol is visible for that viewport.
You can move around the canvas using one of the following methods:
To select objects, switch to Select mode (keyboard shortcut: Esc), then click the desired object.
To select a pin, you might need to click twice (but not double-click). The first click is to select the parent object, the second click actually selects the pin.
Select multiple objects by hold Ctrl while clicking desired objects.
Clicking-and-dragging also selects multiple objects.
To select an object that is overlapped (covered) by others, right click where the object is, click Select.
Hover over menu items to highlight the each object. If your desired object is highlight, click that menu item.
After an object is selected, its attributes are available in the right sidebar for editing.
Arrange tab
Style tab
To move the selected object, drag it to the new position. Or press the arrow keys: up, down, left, right.
To resize the selected object, drag its resize handlers.
Selected object(s) can be cut/copied/pasted. Undoing and Redoing are also supported.
Save your symbols with Save or Save As depending on your need.
Find your symbols in My Symbols dialog.
You can sort symbols by name or by update date.
Click a symbol in the list to preview.
To delete a symbol:
Your symbols will be available to be placed in the schematic under User Library --> My Custom Symbols.
Click-to-place or drag-to-place the symbol to the schematic as usual.